Technical FAQs

Ask a Question

How to configure the logout option from Citect`s runtime screen when the system is idle for some time.

There is LogoutIdle() parameter available in Citect`s INI file. If the current user does not execute any command 
within the specified idle time, a prompt is displayed. If the prompt is ignored, then the user is logged out.
For every user to have the same idle time, you would call this function at startup. Otherwise, you can call
the function from the Users database to specify an idle time for each user. This function will not log out an
automatically logged on user.
For using this you have to put this function in the startup code in the computer setup wizard as shown below,

This will logs the user out after 1 minute.
Was this helpful?
What can we do to improve the information ?