Technical FAQs

Ask a Question

What is the factory default pulsed output settings for the PM810/700/750 Meters.

 The factory default pulse output settings for the PM700/750/810 meters are as follows;
1. Pulse output duration is 100 mSec.
2. Pulse weight is 1kWh / pulse
Was this helpful?
What can we do to improve the information ?