Technical FAQs

Ask a Question

How to reset PM700 kWh (Real Energy Consumption) register to zero remotely using Modbus register by writing Code Command.

To reset the kWh (Real Energy Consumption) register to zero remotely using Modbus register procedure is as follow;
 
1)    Write the value "0" to both register 7016 and 7017
2)    Write the value "6209" to register 4126.
Was this helpful?
What can we do to improve the information ?