Technical FAQs

Ask a Question

Is it possible to change the scaling of Voltage from V (Volt) to MV (Megavolt) on the display of PM750.

The scaling of Voltage at the display of PM750 is changed automatically by the meter as per the Voltage level of the supply.
The PM Meter will change the Display scaling. It is not possible to change it manually.
Was this helpful?
What can we do to improve the information ?