Technical FAQs

Ask a Question

How many devices can be connected on the expansion bus of Modicon M168 Controller.

The Maximum number of devices  that can be connected on the expansion bus of Modicon M168 Controller.
 
1- 32 Devices if the Baud Rate = 20k bits/seconds.
 
2- 8 Devices if the Baud Rate = 500k bits/seconds.

Refer attached file for more information,
Was this helpful?
What can we do to improve the information ?