Technical FAQs

Ask a Question

Is it possible to install external earth-fault module GFP of Compact/Easypact CVS MCCB with Easypact EZC MCCB range.

The external earth-fault module GFP of Compact/Easypact CVS MCCB cannot be installed with Easypact EZC MCCB.
It can be intsatlled with Compact /Easypact CVS/Compact NSX MCCBs only.

Please refer the below selection chart :



Note: Kindly order one number of Shunt Trip coil along with one Ground fault protection module for CVS 100 to 630.
           Order one Auxilary contact alongwith Shunt coil for CVS800.
Was this helpful?
What can we do to improve the information ?