Technical FAQs

Ask a Question

What is the rated service breaking capacity Ics of C60 UL1077 range of MCB.

AS per IEC 60947, the Ics value of the circuit breaker is in terms of the % of ICU rating. The Ics value of the
C60UL 1077 offer is equal to 75% of Icu rating.
Was this helpful?
What can we do to improve the information ?