Technical FAQs

Ask a Question

What is the contact gap for the C60 range MCB when the breaker is Open.

The gap between the contacts for the C60 range when the breaker is open is minimum = 5.5 mm, For
your information the standard requires 4 mm.
Was this helpful?
What can we do to improve the information ?