Technical FAQs

Ask a Question

What is the maximum breaking Time value for the C60 range MCB.

The breaking time of the MCB is 3 to 5 second at the time of short circuit. However if the shunt trip release MX
is used with MCB, this MX release also take the 18ms power circuit breaking time.
 
Refer the attached sheet for the details.
Was this helpful?
What can we do to improve the information ?