Technical FAQs

Ask a Question

Is it possible to use the LUCA/LUCB control unit of Tesys U starter in single phase application.

LUCA standard or LUCB advanced control unit of Tesys U is designed for 3 phase application. These units have the phase
imbalance feature and it can not be deactivated. If this unit will be use on a single phase then this unit got tripped due to the
phase imbalance.
SO if the application is single phase, then take the LUCC** or LUCM** control units with Tesys U starter.
Was this helpful?
What can we do to improve the information ?