Technical FAQs

Ask a Question

Is the Profibus-DP LULC07 communication module compatible with the Tesys U LUTM controller.

The Profibus-DP LULC07 communication module is not compatible with TeSys U motor controller LUTM.
This LULC07 is only compatible with Tesys U LUB**/LU2B** motor starter.
Was this helpful?
What can we do to improve the information ?