Technical FAQs

Ask a Question

Is TeSys U suitable for DC Motor applications.

All control unit of Tesys U are designed for AC load applications only.Due to the TeSys U design specifications
and accessories limitations, it is not allowed to use Tesys U on DC load.
Was this helpful?
What can we do to improve the information ?