Technical FAQs

Ask a Question

Is it possible to use Tesys T for people protection as residual current protection device.

TesysT cannot be used for people protection even if the level of detection for earth fault is very low.This product has not
be tested and designed regarding earth fault for people protection (time of tripping when the ground fault threshold is measured).
Was this helpful?
What can we do to improve the information ?