Technical FAQs

Ask a Question

What is the part number for the fiber cable used between the Primary and Standby CPU's in a Unity Hot Standby application, Is this cable included in my purchase of the HSBY processor.

This cable is not included in your purchase of the 140CPU671 60. The part number(s) of the fiber MT/RJ cable are,

490NOR0003      3 m MTRJ/ MTRJ
490NOR0005      5 m MTRJ/ MTRJ
490NOR0015      15 m MTRJ/ MTRJ
Was this helpful?
What can we do to improve the information ?