Technical FAQs

Ask a Question

Is it possible to run the motor in reverse direction by using Altistart 48 Soft Starter.

Yes, it is possibleto run the motor in reverse direction by using Altistart 48 Soft Starter. Refer to attached file for wiring scheme.
Was this helpful?
What can we do to improve the information ?