Technical FAQs

Ask a Question

How many communication ports are inbuilt in Altivar 212 Drive.

Two communication ports are inbuilt in Altivar 212 drive.
It enables simultaneous connection to a communication network and an HMI terminal.
 
Refer to attached file for more detail of communication port.
Was this helpful?
What can we do to improve the information ?