Technical FAQs

Ask a Question

What is forced & fire functions in Altivar 212 Drive.

This function is used to force the speed enable in case of emergency
(Fire, smoke extraction …) and NOT stop the drive and motor.
Refer to attached file for more detail of forced & fire functions.
Was this helpful?
What can we do to improve the information ?