Technical FAQs

Ask a Question

What are the main differences between standard Harmony XACA and Harmony XACA…H7 Pendant Control Station Enclosures.

Main differences between Standard Harmony XACA and Harmony XACA…H7 Pendant Control Station Enclosures is as below.
 
 
1.The Harmony XACA*H7(UL)Pendant Control Station Enclosures have a yellow central part instead of black as compared to
standard Harmony XACA Pendant Station Enclosures.
 
2.Harmony XACA*H7(UL)Pendant Control Station Enclosures have plastic material composition which are not the same like that
of
polypropylene used in standard Harmony XACA Pendant Station Enclosures,but their yellow colors are very closed.
Was this helpful?
What can we do to improve the information ?