Technical FAQs

Ask a Question

Which of Diameter 40mm Push Emergency Stop Pushbuttons are suitable for base mounting for Harmony XACA and XACB Pendant Control Stations.

Diameter 40mm Push Emergency Stop Pushbuttons suitable for Base Mounting for Harmony XACA and XACB Pendant Control Stations:
 
1.ZA2BS844(Trigger action latching Emergency stop pushbutton with Diameter of push 40mm,Turn to release,Red Colour).
 
2.ZA2BS944(Trigger action latching Emergency stop pushbutton with key release(n°455),key withdrawal in reset with
   Diameter of push 40mm,Red Colour).
Was this helpful?
What can we do to improve the information ?