Technical FAQs

Ask a Question

What accessories necessary to obtain Ethernet Network Communication for PM850.

In order to connect the PM850 to the network Ethernet you have two options, the first being that you can purchase a newly
developed PM8ECC that connects directly to the back of the PM850 or you can use an EGX100 or EGX300.
Was this helpful?
What can we do to improve the information ?