Technical FAQs

Ask a Question

What is the duration used to determine sag/swell event in PM870.

The PM870 is able to detect sag and swell events less than 1/2 cycle duration.
Was this helpful?
What can we do to improve the information ?