Technical FAQs

Ask a Question

Is there any test kit available for testing of Masterpact MVS ACB trip units.

There is a basic recommendation of testing the Masterpact MVS trip units by using Hand Held Test Kit, the ordering code is 33594.
The Hand held test kit may be used:
  • Check operation of the control unit and the tripping and pole opening system by sending a signal simulating a short circuit.
  • Power source : standrad LR6 AA battrey.
Was this helpful?
What can we do to improve the information ?