Technical FAQs

Ask a Question

Is there any accessory available through which we can retrieve the electrical data from micrologic trip unit in Masterpact NW/NT ACB.

GetnSet is a portable data acquisition and storage accessory that connects directly to the Micrologic control units of Masterpact circuit breakers to read important
electrical installation operating data and Masterpact protection settings.This information is stored in the GetnSet internal memory and can be transferred to a PC
via USB or Bluetooth for monitoring and analysis.
 
The ordering Ref. no. for this unit is 48789.

Was this helpful?
What can we do to improve the information ?