Technical FAQs

Ask a Question

How may breakers/Micrologic can be connected with one AD module.

It is confirmed that all tests has been done only in the configuration of 1 AD module with 1 Micrologic. You can connect BCM, CCM
module on the same AD module.
if more micrologic is connected on one AD module, more the capacitive effect between wires of the 24VDC and the ground is significant.
In that condition, the flow of HF common mode current from 24V DC to the ground through the capacitive effect will be able to create more
disturbances. The AD module is dedicated for Micrologic and it is strongly recommended do not use this 24Vdc for another purpose.
Was this helpful?
What can we do to improve the information ?