Technical FAQs

Ask a Question

Which type of RCCB is suitable for inverter load.

For inverter load application, “Si" type RCCB can be used which will work in the application of loads with electronics & rectifiers. 
"Si" RCCB can be used in AC as well as Pulsated DC network.
Was this helpful?
What can we do to improve the information ?