Technical FAQs

Ask a Question

What is the purpose of Program Loader TM2USBABDEV1 for Modicon M238 Controllers.

 The TM2USBABDEV1 program loader is an accessory which is designed to simplify updating or duplication of applications on
 Modicon M238 logic controllers without the need for a programming terminal.
1.For updating an application generated by SoMachine, stored on a USB memory stick, will be transferred by the program
   loader to an M238 controller.
2.For duplication where an application is transferred from an M238 controller to the program loader.The application is stored
  on a USB memory stick, then transferred from the program loader to another M238 controller.
Was this helpful?
What can we do to improve the information ?