Technical FAQs

Ask a Question

How many High Speed Counter(HSC)channels can be configured in Modicon M238 Controller and what is maximum frequency.

Modicon M238 Controller allows maximum 8 numbers of High Speed Counter(HSC)channels with maximum frequency 100Kz.
It allows counting pulses and update outputs regardless of the scan time of the application.
A Simple counter uses one channel.
A Main counter uses 4 channels.
HSC channel numbers
Up 8 configured in “Simple Counter”.
Up 4 Simple counter and 1 “Main Counter”.
Up 2 configured in “Main Counter” .
Was this helpful?
What can we do to improve the information ?