Technical FAQs

Ask a Question

What is CANmotion principle and many axis can be synchronized by Modicon LMC058 Controller.

The Modicon LMC058 Motion Controller has two CAN connections allowing user to declare either a CANmotion master
 and a CANopen master or two CANopen masters:
 
1.One connection (CAN1)supports a CANopen manager or a CANmotion
Manager and it is able to synchronize up to 8 devices (Lexium 05, Lexium 32 Servo and Lexium SD3 Stepper Drive) on CANmotion.
 
2.The other (CAN0) only supports a CANopen manager, which does not support motion devices.
 
Refer to attached document for Canmotion Principle.
Was this helpful?
What can we do to improve the information ?