Technical FAQs

Ask a Question

If the battery 990XCP98000 is connected in 140CPU67160 and CPU is not powered on. How long will it take to drain the battery.

Battery load @ Power off is 420 micro Ampere and service life is 1200mAH.
So 1.2 /420 micro Ampere is around 2857 Hours i.e. around 4 months.
Was this helpful?
What can we do to improve the information ?