Technical FAQs

Ask a Question

In Unity Pro where IO status bytes are configured for Quantum PLC.

Double click the Remote IO Quantum Drop and in the “Config” Tab provide the Starting address of the Status Table and Ending Address of the Status table.
The status tables are configured for each remote IO drop.

Was this helpful?
What can we do to improve the information ?