Technical FAQs

Ask a Question

The MAC ID of the STB NIC2211 is 00 00 54 10 01 02. What is the default IP address.

The MAC ID is given in the hexadecimal format. For STB NIC2211 we need to convert this hexadecimal directly to decimal to get the
default IP address. In this case the IP address would be 84.16.01.02.
Was this helpful?
What can we do to improve the information ?