Technical FAQs

Ask a Question

What is the operation of AI2F [AI2 filter] parameter in Altivar 61/71 drive.

This filter is like a Low Pass Filter and can be set from 1 to 10 seconds, 10 seconds get better immunity.
It can filter out the sudden changes or frequency perturbations on the analog input terminal.
Was this helpful?
What can we do to improve the information ?