Technical FAQs

Ask a Question

The letter L or H is flashing on the display of my ATV212

The letter L indicates that the Motor is going into Overload this needs to be investigated as there could be a problem with the motor or the drive system
The letter H indicates that the drive is approaching it’s over heat fault setting and the drive should be check to see what is causing its heating up. Make sure that all the filters are cleaned and there is no obstructions to the air flow and that the fans on the drive are working
Was this helpful?
What can we do to improve the information ?