Technical FAQs

Ask a Question

What is the frequency for Illuminated beacon reference XVBL8B4.

The Frequency of the illuminated Beacon unit,Red colour with 10 Joule “flash” discharge tube XVBL8B4 with 24VDC supply will depend on the temperature.
At 25°C and 55°C,below are the Frequencies Tolerance Ranges:
At 25°C    0.67Hertz< F < 2Hertz<==> 0.5seconds < T < 1.5seconds
At 55°C    0.5Hertz < F < 1.25Hertz <==> 0.8seconds < T < 2seconds
T- Time Period.
Was this helpful?
What can we do to improve the information ?