Technical FAQs

Ask a Question

Do we need to purchase Shunt, Closing & UV extra if we are purchasing Motorised NSX MCCB and want to close & trip the MCCB remotely

Motorised NSX MCCB comes with closing and shunt as default which are mounted inside the motor mechanism. You need to purchase the UV separately
Was this helpful?
What can we do to improve the information ?