Technical FAQs

Ask a Question

How to Upload or Download files to M258 Controller with USB Memory Key.

The Modicon M258 Logic Controller allows file transfers with a USB memory key. Using this USB Memory key,it is
not necessary to use SoMachine or FTP Server.
 
To upload or download files to Modicon M258controller with a USB memory key,use one of the following methods:
 
1.The clone function(Use of an Empty USB Memory Key).
 
2.A script stored in the USB Memory Key .
 
When a USB memory key is inserted into the USB Data Port of the Modicon M258 controller,the firmware searches and
executes the script contained in the USB memory key (/sys/CMD/Script.cmd).
Was this helpful?
What can we do to improve the information ?