Technical FAQs

Ask a Question

What are the screw size and wire size for the CT and PT terminal connections on the PM820 and PM850 meters.

The terminal screws are 6-32 standard screws. Each meter is supplied with spade lugs that
accommodate 14-16 AWG wire.
Was this helpful?
What can we do to improve the information ?