Technical FAQs

Ask a Question

Is it possible to connect two nos of FDM121 with same Compact NSX in ULP System.

The Intelligent Modular Unit (IMU) contains a maximum of one ULP module of any given type.
The IMU cannot contain more than one front display module FDM121 or more than one Compact NSX circuit breaker.
Was this helpful?
What can we do to improve the information ?