Technical FAQs

Ask a Question

What is the consumption of the electric motor for a Compact NS 250 at the time of opening.

For DC's EMV the duty cycle is different according to the voltage of the power supply.
 
For DC motors
Nominal consumption on motor
Duty cycle
Electric's consumption
 EMV 24/30VDC
500 VA
63 %
315VA
 EMV 48/60VDC
500 VA
78 %
390VA
   EMV 100/130VDC
500 VA
77 %
385VA
   EMV 200/250VDC
500 VA
71 %
355VA
 
For AC's EMV we have always duty cycle at 50% so 500VA x 0.5 = 250 VA

For AC motors
Nominal consumption on motor
Duty cycle
Electric's consumption
EMV 48/60VDC
500 VA
50 %
250 VA
 EMV 110/277VDC
500 VA
50 %
250 VA
 EMV 380/480VDC
500 VA
50 %
250 VA
 
 
Was this helpful?
What can we do to improve the information ?