Technical FAQs

Ask a Question

What is the meaning of ‘Evn 1’ in the setup table of the DM6000 and PM1000 series meters.

The 1st three letters shows the selected parity (‘Evn’ for even, ‘Odd’ for odd or ‘no’ for no parity) and the last
digit of the same row shows the selected stop bit of the communication.
Was this helpful?
What can we do to improve the information ?