Technical FAQs

Ask a Question

What is the air flow rate of the Fan for the Altivar 32 drive.

Refer the below chart forair flow rate of each Altivar 32 drive.

  380V / 500V 3PH                  
Power rating 0,37kW 0,55/0,75kW 1,1/1,5kW 2,2kW 3kW 4kW 5.5kW 7.5kW 11kW 15kW
                     
Air flow m3/min 0.24 0.24 0.24 0.45 0.45 0.45 1.32 1.32 3.2 3.2
                     

  200V 1PH        
Power rating 0,18kW 0,37kW 0,55/0,75kW 1,1/1,5kW 2,2kW
           
Air flow m3/min 0.24 0.24 0.24 0.45 0.45
           


Was this helpful?
What can we do to improve the information ?