Technical FAQs

Ask a Question

What is the detail of the error AL3F1 error on Lexium 23D/A.

AL3F1 means Pr command overflows
An absolute positioning command has been executed after a position command counter overflow.
Check: Verify that absolute positioning will not lead to a position that is out of range when executing
            absolute positioning command.
Was this helpful?
What can we do to improve the information ?