Technical FAQs

Ask a Question

What is the maximum operating altitude for Altivar 32 drive.

Up to 1000 Meter without derating.
1000...3000 Meter, derating the current by 1 % per additional 100 M.
Was this helpful?
What can we do to improve the information ?