Technical FAQs

Ask a Question

What are the different ways of connecting expansions to M218 Controller.

The 3 ways for connecting expansions to M218 controller are by:
 
1.Directly connected expansions.
2.Expansions with interface.
3.Mixed type of expansions.
 
Refer to attached document for pictorial information for different ways of connecting expansions to M218 Controller.
Was this helpful?
What can we do to improve the information ?