Technical FAQs

Ask a Question

What minimum clearance is required during installation of Modicon M218 Controller.

The Modicon M218 Logic Controller has been designed as an IP20 product and must be installed in an enclosure.Refer 
to attached document for the minimum clearances that must be respected when installing Modicon M218 controller.
Was this helpful?
What can we do to improve the information ?