Technical FAQs

Ask a Question

What is the UL file and conditions of acceptability for Multi 9 UL 1077 Recognized C60 Supplementary Protectors?

UL 1077 Circuit Breaker, File No. E90509, CSA C22.2 No. 235 File No. 179014

CONDITIONS OF ACCEPTABILITY (NOT FOR UL REPRESENTATIVE USE):
Use - For use only in products where the acceptability of the combination is determined by Underwriters Laboratories Inc.

1.These devices are intended to be DIN rail mounted or faceplate mounted with front mounting bracket accessory. Additionally, they should be mounted in an enclosure having adequate strength and thicknesses in the intended manner and with spacing in accordance with the requirements of the overall equipment.

2.  Intentionally left blank.

3.These devices should be used within their Recognized ratings.

4.Test records should be reviewed, including short circuit tests, when judging the acceptability of these devices in an end use application.

5.These devices are not suitable for branch circuit protection.

6.These devices are designed to trip within the trip curve characteristics provided by the manufacturer; as indicated in the report.  Trip times were confirmed at 300% of rating and at 150% of rating.

7.Considerations should be given to the need for insulating barriers when uncovered openings in the side of the case are mounted adjacent to metal surfaces, such as an enclosure.

8.These devices have been determined to be trip free per
requirements effective July 14, 2008, 6th Edition of UL 1077.

9.The terminals are suitable for Field or Factory wiring.
Was this helpful?
What can we do to improve the information ?