Technical FAQs

Ask a Question

How to resolve Vijeo Frame application error,while trying to open VijeoDesigner project from SoMachine Software.

The Vijeo Frame Application Error occur because one DLL (Dynamic link library)is not registered correctly in
the Windows System after the installation of a patch.
The solution would be to execute the following
command (in the "RUN" window of Windows- Regsvr32 "%SystemRoot%\system32\msxml3.dll".This will register
the DLL again and user would be able to open VijeoDesigner application normally from SoMachine Software.
Was this helpful?
What can we do to improve the information ?