Technical FAQs

Ask a Question

How to resolve error message when trying to add the SysTime library to the project "The process cannot access the file because it is being used by another process".

The Error Message "The process cannot access the file because it is being used by another process"pops up,if user want
to install a library and the source of the library is in the same folder where SoMachine tries install it.
New libraries should be placed on a temporary folder and then installed by using device repository to have the libraries installed
in the correct path.
 Refer to attachment where user can see which setting of the system that should be adapted to get the Device and Library Repository
back to the tools tab in SoMachine Software.
Was this helpful?
What can we do to improve the information ?