Technical FAQs

Ask a Question

What operating systems are supported by Advantys Configuration software Version V5.5.0.

Advantys Configuration Software can be installed on different Windows platforms using the same setup package. The setup will
detect the platform and the specific installation requirements automatically. The following Windows platforms are supported:
·        x86 Windows XP Professional Service Pack 3
·        x86 Windows Vista Business and Ultimate
·        x86 Windows 7 Professional, Ultimate and Enterprise
·        x64 Windows 7 Professional 
In addition, the following system components are required:
·        Windows Installer V3.0 ¹) and above
·        Internet Explorer 6.0 and above
·        Microsoft .Net Framework 2.0 (included in setup)
Was this helpful?
What can we do to improve the information ?