Technical FAQs

Ask a Question

What are the purposes of two USB Ports in Modicon M258 Controller.

Below are the puposes of two standard USB ports:
 
1.Mini-USB B port for SoMachine programming software.
 
2.USB-A port for memory key for program,firmware,data files transfer at the speed of 480 Mega bits/second.
Was this helpful?
What can we do to improve the information ?